Contact an Expert

Thread: proramming/ remote operation using Matlab for Hp 8753C network analyzer ???


Permlink Replies: 0 - Pages: 1
umerfarooque001

Posts: 5
Registered: 04/03/12
proramming/ remote operation using Matlab for Hp 8753C network analyzer ???
Posted: Jun 7, 2012 1:49 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I have a task to complete on hp 8753C network analyzer . . I would like

1. to measure absolute power for three different receiver data on the three receiver channel available A, B, R . . . is that possible ??

2. I would like to control analyzer remotely using Matlab, typically i would like to setup measurement/read trace data etc. in Matlab . . .??

C. Is SCPI language supported on 8753C??? If not, which language is supported and please send link/document for details on this??? from where I will have driver downloaded for remote operation from matlab ???

It is requested to provide in details and step-by-step so that I can do it easily . . . I have done only a little work on PNA 8362B .. . . . .

Thanks a lot
Umer Farooque

Point your RSS reader here for a feed of the latest messages in all forums