Contact an Expert

Thread: EMmodel ERROR


Permlink Replies: 1 - Pages: 1 - Last Post: May 31, 2012 10:24 AM Last Post By: MARCP Threads: [ Previous | Next ]
sergi

Posts: 4
Registered: 04/17/12
EMmodel ERROR
Posted: May 31, 2012 3:30 AM
Click to report abuse...   Click to reply to this thread Reply
Hi everyone!

I'm trying to create an ADS component of my EMPro design. I've followed all the steps that appear on the documentation, section Exporting EMPro Simulation Results as emModel. When I try to simulate the model with ADS it stops and shows the error:


Simulation / Synthesis Messages

Error detected by hpeesofsim during SP analysis `SP1'.
COMPONENT `I__2.em_data':
Invalid citi-data in the EM Model database.
Error detected by hpeesofsim during SP analysis 'SP1'.
Fatal error occurred while evaluating model `MomCmpt', instance `I__2.em_data'.

Status / Summary

hpeesofsim (*) 372.600 Nov 12 2011 (built: 11/11/11 19:49:29)
Copyright Agilent Technologies, 1989-2011.

SP SP1[1] <butterworth2_lib:cell_1:schematic> freq=(2 GHz->4 GHz)
.
******************************************

          • Abnormal Simulator Termination *****
******************************************
The simulator has unexpectedly terminated.


The strange thing is that when I generate the emModel from another design, like the Microstrip 50 ohm example, it works perfectly, so I don't have any idea on what is happening.
Thanks all!

Sergi
MARCP

Posts: 28
Registered: 06/08/09
Re: EMmodel ERROR
Posted: May 31, 2012 10:24 AM   in response to: sergi in response to: sergi
Click to report abuse...   Click to reply to this thread Reply
Hi Sergi,

It would be best to contact Agilent tech support to debug the specific problem with your project.

eesof_support@agilent.com

Thanks,
Marc

Point your RSS reader here for a feed of the latest messages in all forums