Contact an Expert

Thread: DSO1000A


Permlink Replies: 1 - Pages: 1 - Last Post: May 24, 2012 7:17 AM Last Post By: algoss
sgagnon

Posts: 1
Registered: 05/23/12
DSO1000A
Posted: May 23, 2012 1:45 PM
Click to report abuse...   Click to reply to this thread Reply
I'm stcuk in front of a "frozen" DSO1024A in the dual trigger mode.
No matter what button I push, if I turn the scope ON and OFF and ON or unplug it it remain frozen.
The values around the monitor are displayed ( trigger, sensivity ... ) but no trace are on the display.
No matter what button I push, the keyboard is dead.

Any way I kick it back to life, some type of BIOS MASTER RESET ??

( The bios is up to date, it's a new acquisition and had been running perfectly for the last 5 month )
algoss


Posts: 636
Registered: 11/03/06
Re: DSO1000A
Posted: May 24, 2012 7:17 AM   in response to: sgagnon in response to: sgagnon
Click to report abuse...   Click to reply to this thread Reply
It's probably something like a stuck button, or a loose cable. Resetting the BIOS probably won't help, since that happens on every power-up. Did the scope work at one point, then stop? If you shake it, is there anything loose inside?

I would suggest some light to moderate "percussive maintenance". If that doesn't work, a repair is in order.

Al

P.S. Percussive Maintenance involves shaking, tapping, hitting and/or slapping the HW

Point your RSS reader here for a feed of the latest messages in all forums