Contact an Expert

Thread: How to use Network Analyzer test insertion loss


Permlink Replies: 4 - Pages: 1 - Last Post: Jun 1, 2012 1:02 AM Last Post By: Dr_joel
pdf001

Posts: 3
Registered: 05/22/12
How to use Network Analyzer test insertion loss
Posted: May 22, 2012 2:38 AM
Click to report abuse...   Click to reply to this thread Reply
I'm new for this.
I want to test insertion loss of a relay in close state.Do I need to make a special wire for test?
Can nerwork analyzer test crosstalk and isolation for relay?How to test
am95405


Posts: 212
Registered: 12/05/05
Re: How to use Network Analyzer test insertion loss
Posted: May 22, 2012 8:18 AM   in response to: pdf001 in response to: pdf001
Click to report abuse...   Click to reply to this thread Reply
Hello,

You certainly can use a network analyzer for testing either insertion loss or isolation/crosstalk (closed or open states) of a relay or switch.

Which piece of Agilent test equipment are you using? If you give us the specific model, perhaps we can point out sections of the manuals that would be helpful.

Also, is your device connectorized? You'll need to calibrate out the other wires or test fixtures, so you can just see the performance of your relay.

If N9912A or N9923A's CAT mode, you measure insertion loss, and perform a normalization calibration.

If N9923A or other VNA's with S-parameters, you measure S21 or S12, and can perform a normalization or full 2-port calibration.

Depending on the loss or isolation you are measuring, you may need to lower the IFBW to reduce the noise level and improve the dynamic range.

Afsi Moaveni
pdf001

Posts: 3
Registered: 05/22/12
Re: How to use Network Analyzer test insertion loss
Posted: May 25, 2012 2:16 AM   in response to: am95405 in response to: am95405
Click to report abuse...   Click to reply to this thread Reply
Thank U
traducere simul...


Posts: 2
Registered: 05/23/12
Re: How to use Network Analyzer test insertion loss
Posted: May 30, 2012 12:56 AM   in response to: pdf001 in response to: pdf001
Click to report abuse...   Click to reply to this thread Reply
Hi i am new to this topic as well as to this site and would appreciate any information regarding Network Analyzer.
______________________________
traducere simultana

Edited by: traducere simultana on Jun 1, 2012 1:01 AM
Dr_joel


Posts: 2,788
Registered: 12/01/05
Re: How to use Network Analyzer test insertion loss
Posted: May 30, 2012 9:18 AM   in response to: traducere simul... in response to: traducere simul...
Click to report abuse...   Click to reply to this thread Reply
look at the pdfs here for lots of information: http://bit.ly/NefIjJ

Point your RSS reader here for a feed of the latest messages in all forums