Contact an Expert

Thread: How convert manually board files unix to windows


Permlink Replies: 4 - Pages: 1 - Last Post: Mar 2, 2014 1:17 PM Last Post By: tamusino Threads: [ Previous | Next ]
jolumo1

Posts: 3
Registered: 02/10/11
How convert manually board files unix to windows
Posted: May 14, 2012 8:13 AM
Click to report abuse...   Click to reply to this thread Reply
Can I help me? I need convert board files of unix to windows manually , because with agilent convert tools it board do not pass ipg.

regards

oconnellj

Posts: 95
Registered: 03/06/09
Re: How convert manually board files unix to windows
Posted: May 18, 2012 6:05 AM   in response to: jolumo1 in response to: jolumo1
Click to report abuse...   Click to reply to this thread Reply
Hi, what problems have you had with IPG?

if it passes IPG on Unix - this is place to start - so first make a copy of the directory to another 'safe' directory location where it doesnt matter if you make a mistake > then run IPG and make sure it passes on UX

another thing that helps, is if you are at software revision 05.21 on Unnix and then you can convert any tests to use the PC style delimiter which uses a '%' instead of ':' as seperator for the parent:child type tests (i.e. panel tests, diodes resistor packs etc..)

this is done my using 'enable common delimiter' in board config and you can then convert your test programs on Unix to the new file seperation - it makes transition much easier from UX to PC

main problem you will face initially is the different library path structure, because it is no longer /hp3070 etc,, , it is C:/Agilent_ICT... - this is main area for issues and needs to be corrected in the board file and any calls to data logging in tetsplan etc.., and also missing library files objects - apart from that transition is straightforward, and is MUCH easier if you can get to use the new delimiter structure on UX before swapping over
jolumo1

Posts: 3
Registered: 02/10/11
Re: How convert manually board files unix to windows
Posted: May 19, 2012 8:51 AM   in response to: oconnellj in response to: oconnellj
Click to report abuse...   Click to reply to this thread Reply
Thanks for you answer.
I convert : to % manually , and it work fine.
RobMx

Posts: 1
Registered: 05/30/12
Re: How convert manually board files unix to windows
Posted: May 30, 2012 7:48 PM   in response to: jolumo1 in response to: jolumo1
Click to report abuse...   Click to reply to this thread Reply
I had the same problem a few months and what I did to fix it was to develop my own "conversion tool". This was the only way to make the conversion because I have to migrate a lot of programs with the same problem.

If you need help in the future maybe I could help.
tamusino


Posts: 2
Registered: 07/28/12
Re: How convert manually board files unix to windows
Posted: Mar 2, 2014 1:17 PM   in response to: RobMx in response to: RobMx
Click to report abuse...   Click to reply to this thread Reply
I have a similar problem can you share your conversion tool, I need to convert several files.
Thanks
Regards

Point your RSS reader here for a feed of the latest messages in all forums