Contact an Expert

Thread: EXA: N9010A Roadmap


Permlink Replies: 1 - Pages: 1 - Last Post: May 18, 2012 9:36 AM Last Post By: tabbott
obranje

Posts: 16
Registered: 09/15/10
EXA: N9010A Roadmap
Posted: May 17, 2012 4:03 PM
Click to report abuse...   Click to reply to this thread Reply
Dear All,

Do you know why this Serie does not have the Tracking Generator Option? Is this going to be available in the future?

Thanks you,
Oscar
tabbott


Posts: 1,483
Registered: 07/24/09
Re: EXA: N9010A Roadmap
Posted: May 18, 2012 9:36 AM   in response to: obranje in response to: obranje
Click to report abuse...   Click to reply to this thread Reply
Hi Oscar -

The tracking generator option is currently only available on the N9000A CXA.

However, the external source control option (Option ESC) is available on the EXA which enables the EXA to control the MXG or PSG signal source for stimulus-response tests.

The tracking generator functionality in many cases can be achieved by the EXA with option ESC and a signal source.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums