Contact an Expert

Thread: How to remote trigger a generator with a E5818A


Permlink Replies: 4 - Pages: 1 - Last Post: Jun 22, 2012 12:36 AM Last Post By: Tardz Threads: [ Previous | Next ]
cqq

Posts: 3
Registered: 05/14/12
How to remote trigger a generator with a E5818A
Posted: May 15, 2012 12:49 AM
Click to report abuse...   Click to reply to this thread Reply
For an application I have a generator (E8257) on a remote location. This generator must generate a couple of discrete frequencies when triggered.

To trigger the generator I use a E5818A Trigger Box. With the use of the "Interactive LXI" program I can generate a manual trigger on TTL1 of the E5818A Trigger Box. Command to the E5818A are send via LAN.

What VISA commands I have to send to the E5818A trigger Box to configure it for generating a trigger via LAN on TTL1? And what VISA command does generate the trigger on TTL1? The E5818A manual does not provide me with enough information.
cqq

Posts: 3
Registered: 05/14/12
Re: How to remote trigger a generator with a E5818A
Posted: May 25, 2012 5:13 AM   in response to: cqq in response to: cqq
Click to report abuse...   Click to reply to this thread Reply
Why is the post moved from generators to Power Meters?

An E8257 is a generator and an E5818A is a trigger box both have nothing to do with power meters and sensors.
iandoubleyou


Posts: 56
Registered: 02/07/07
Re: How to remote trigger a generator with a E5818A
Posted: May 25, 2012 8:01 AM   in response to: cqq in response to: cqq
Click to report abuse...   Click to reply to this thread Reply
Not sure why this was moved - but I put it back in it's rightful place.
tabbott


Posts: 1,483
Registered: 07/24/09
Re: How to remote trigger a generator with a E5818A
Posted: May 30, 2012 9:38 AM   in response to: iandoubleyou in response to: iandoubleyou
Click to report abuse...   Click to reply to this thread Reply
Hi -

Creating delay using E5818A, periodic, or N-cycle trigger pulses from a single trigger often requires custom circuitry or pulse generator.

Refer to the programming example page 121/135 from the link http://www.home.agilent.com/agilent/redirector.jspx?action=ref&cname=AGILENT_EDITORIAL&ckey=1400328&lc=eng&cc=MY&nfr=-11143.0.00&pselect=SR.GENERAL

The Syntax used as below:
TRIGger:TTL1|2:SOURce <source_value>
TRIGger:TTL1|2:SOURce?

And the examples as below
TRIG:TTL1:SOUR ”EXT1”

This command sets the trigger event TTL1 source to “EXT1”
TRIG:TTL1:SOUR?

This query will request for the source of trigger event TTL1

I hope this helped -
Tardz

Posts: 45
Registered: 11/08/07
Re: How to remote trigger a generator with a E5818A
Posted: Jun 22, 2012 12:36 AM   in response to: tabbott in response to: tabbott
Click to report abuse...   Click to reply to this thread Reply
Hi, I have same problem, I'm trying to generate a pulse on TTL1 port based on LAN without success.

If I use commands TRIG:TTL1:SOUR 'EXT1' and send a pulse on EXT1 input, I have a pulse at TTL1 output. At this point everything is ok.

Now if I sent command TRIG:TTL1:SOUR 'LAN0' and send command TRIG:TTL1:STAT 1, I have no pulse at TTL1 output port.
(this an example from programming manual p8 ou(pdf p20) http://cp.literature.agilent.com/litweb/pdf/E5818-90005.pdf )
Which command I need to generate a pulse on TTL1 based on LAN?

Thanks.


Point your RSS reader here for a feed of the latest messages in all forums