Contact an Expert

Thread: Meassuring several connected 2wire resistances (NTC)


Permlink Replies: 1 - Pages: 1 - Last Post: May 14, 2012 2:13 PM Last Post By: tomc
lukeskymuh

Posts: 1
Registered: 05/14/12
Meassuring several connected 2wire resistances (NTC)
Posted: May 14, 2012 10:26 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I am measuring several 5kOhm NTCs with 3x 34901A 20 Channel Multiplexer with a 34970A.
Can I have problems if I connect one side of all sensors together?
I have tested it with 2 sensors and it worked, but is it a reliable solution?

Best Regards
Luke

Edited by: lukeskymuh on May 14, 2012 10:28 AM
tomc

Posts: 218
Registered: 01/12/11
Re: Meassuring several connected 2wire resistances (NTC)
Posted: May 14, 2012 2:13 PM   in response to: lukeskymuh in response to: lukeskymuh
Click to report abuse...   Click to reply to this thread Reply
This works fine as long as you are careful to be sure that there are no extraneous voltages on the NTC leads. In other words, make sure the NTC leads don't make electrical connections to any points where there are significant voltage differences, because when you connect this way eacn NTC no longer has a floating connection to the DMM. You are vulerable to ground loop problems, but as long as you are carefully with the wiring, this should work without problems.

Point your RSS reader here for a feed of the latest messages in all forums