Contact an Expert

Thread: sample VEE program for the synchronized all-states PDL/PER method - updated


Permlink Replies: 0 - Pages: 1 Threads: [ Previous | Next ]
mkelly

Posts: 178
Registered: 02/06/07
sample VEE program for the synchronized all-states PDL/PER method - updated
Posted: May 11, 2012 1:27 AM
Click to report abuse...   Click to reply to this thread Reply
The attached VEE program is a sample for the method described in the application note to make all-states PDL or PER measurements. The sample program only controls the polarization controller (N7785B or N7786B, N7784B N7788B as well) and the power meter. The power meter control uses the 816x Plug&Play driver. The visa address for the power meter will need to be set correctly and the polarization controller is expected on the USB interface. The laser source is not controlled and any stable polarized source can be used with the program.

http://cp.literature.agilent.com/litweb/pdf/5990-9973EN.pdf

Edited by: mkelly on May 11, 2012 2:31 AM
file replaced

Edited by: mkelly on May 11, 2012 3:13 AM
replace file for minor tweak (using factor 4 for rep rate)

Edited by: mkelly on Aug 31, 2012 9:04 AM
Replaced file. Previous version included some temporary diagnostic modifications.

Edited by: mkelly on Aug 31, 2012 9:06 AM

Point your RSS reader here for a feed of the latest messages in all forums