Contact an Expert

Thread: PNA-X PWR I/O Connector


Permlink Replies: 3 - Pages: 1 - Last Post: May 10, 2012 1:40 PM Last Post By: kaon
Vyrl

Posts: 8
Registered: 10/28/11
PNA-X PWR I/O Connector
Posted: Feb 21, 2012 1:22 PM
Click to report abuse...   Click to reply to this thread Reply
I am trying to control an external circuit by setting a voltage on AO1 on the PWR I/O connector. I am set up for an external trigger and change stimulus on my DUT, then supply the trigger to take a sweep. When set up to use the external trigger in this way, it appears that the voltage on AO1 is never updated. If I change the trigger to internal so that the PNA is constantly sweeping, then the voltage on AO1 does appear to change. Is there a way to update the voltage on AO1 while being externally triggered?
Dr_joel


Posts: 2,775
Registered: 12/01/05
Re: PNA-X PWR I/O Connector
Posted: Feb 21, 2012 3:08 PM   in response to: Vyrl in response to: Vyrl
Click to report abuse...   Click to reply to this thread Reply
If you could be a bit more specific: how do you set the voltage on the AO1? by remote command or front panel interface? Do you set several values or just one or two values? How do you coordinate the setting with the triggering?

BTW, in the next firmware release (scheduled in April), there will be direct control of DC sources (external power supplies) and DC meters, including AO1 so you can set it to trigger each sweep or each point to a different value, or different value for each sweep, or different value on forward and reverse sweep.
Vyrl

Posts: 8
Registered: 10/28/11
Re: PNA-X PWR I/O Connector
Posted: Feb 21, 2012 3:30 PM   in response to: Vyrl in response to: Vyrl
Click to report abuse...   Click to reply to this thread Reply
I'm setting the AO1 voltage using SCPI commands. I did find a command that sets the mode of the AO outputs. CONT:AUX:OUTP1:MOD NOW. This command sets the voltage on the AO1 output immediately. The default sets the voltage after a sweep complete. This command has fixed my problem.

Thank you for the quick response.
Vyrl
kaon

Posts: 1
Registered: 05/10/12
Re: PNA-X PWR I/O Connector
Posted: May 10, 2012 1:40 PM   in response to: Dr_joel in response to: Dr_joel
Click to report abuse...   Click to reply to this thread Reply
As I read it, the direct control on external DC sources is in PNA-x firmware beta release 9.50.09.

When I install the beta firmware, does that update the help file? I need documentation on the SCPI and COM commands for this interface.

Thanks.

Point your RSS reader here for a feed of the latest messages in all forums