Contact an Expert

Thread: Time Domain Analysis


Permlink Replies: 1 - Pages: 1 - Last Post: May 7, 2012 4:40 PM Last Post By: Dr_joel Threads: [ Previous | Next ]
mark2

Posts: 5
Registered: 08/26/11
Time Domain Analysis
Posted: May 4, 2012 3:23 PM
Click to report abuse...   Click to reply to this thread Reply
Good Afternoon,

I am trying to program (using labview) a PNA-X to capture time domain data on the screen.

I use the command calc:tran:time:stat on to turn on the time domain function but I get an error -224 (illegal parameter value) on the analyzer.

Is there another command that is required before I use the above commend?

I can manually turn the transform on and off from the unit, so I know the transform works. Just can't get the program to turn it on.

Any suggestions are welcomed.

thanks

mark
Dr_joel


Posts: 2,793
Registered: 12/01/05
Re: Time Domain Analysis
Posted: May 7, 2012 4:40 PM   in response to: mark2 in response to: mark2
Click to report abuse...   Click to reply to this thread Reply
works for me, but you must first use:
Calc:par:sel "CH1_S11_1" (or whatever the trace name is)

You can always try the commands in the built in command process window to see if the problem is the command or the driving program.

Point your RSS reader here for a feed of the latest messages in all forums