Contact an Expert

Thread: Simulated "Gold Standard" for Time Domain Tuning


Permlink Replies: 4 - Pages: 1 - Last Post: May 3, 2012 6:03 AM Last Post By: mingal Threads: [ Previous | Next ]
mingal


Posts: 110
Registered: 06/08/09
Simulated "Gold Standard" for Time Domain Tuning
Posted: May 1, 2012 9:23 AM
Click to report abuse...   Click to reply to this thread Reply
Howdy-

We wish to tune a "real" filter using simulated data by loading the simulated S-parameters into a VNA and converting them (S11 & S22) from the frequency to the time domain, allowing us to then follow the procedure outlined in e.g. AN 1287-8.

Is this possible? If so, which VNAs are recommended?

Thanks in advance,

Mark W. Ingalls
daras


Posts: 932
Registered: 12/01/05
Re: Simulated "Gold Standard" for Time Domain Tuning
Posted: May 1, 2012 3:08 PM   in response to: mingal in response to: mingal
Click to report abuse...   Click to reply to this thread Reply
With any of the PNA, PNA-X, or ENA analyzers you can load the simulated data in the analyzer in the form of an S2P (touchstone forma) and if you have the time domain option (option 010) on that box, you can perform a time domain transform on the data loaded from the S2P file. There are other ways to do this, but this is the most straight forward and simple approach.
mingal


Posts: 110
Registered: 06/08/09
Re: Simulated "Gold Standard" for Time Domain Tuning
Posted: May 1, 2012 9:25 PM   in response to: daras in response to: daras
Click to report abuse...   Click to reply to this thread Reply
AWESOME! (I thought so, but just wanted to check to be sure.)

Thanks, daras!
Dr_joel


Posts: 2,775
Registered: 12/01/05
Re: Simulated "Gold Standard" for Time Domain Tuning
Posted: May 1, 2012 11:40 PM   in response to: mingal in response to: mingal
Click to report abuse...   Click to reply to this thread Reply
just be sure to use band pass mode in time domain.

And if you are planning to use time domain tuning for manufacturing (rather than R&D), shoot me a pm and we should talk about some other advancements.
mingal


Posts: 110
Registered: 06/08/09
Re: Simulated "Gold Standard" for Time Domain Tuning
Posted: May 3, 2012 6:03 AM   in response to: Dr_joel in response to: Dr_joel
Click to report abuse...   Click to reply to this thread Reply
Dear Dr_joel-

PM sent, because we definitely have production on our minds.

We are also messing about with IFFT(S11(f)) in Agilent's Genesys linear simulator with spotty results.

I have read several of your papers on the topic, but do not feel like I know much yet. I'll keep on it.

mwi

Point your RSS reader here for a feed of the latest messages in all forums