Contact an Expert

Thread: Looking for a 54845A service disk.


Permlink Replies: 4 - Pages: 1 - Last Post: Apr 30, 2012 5:03 PM Last Post By: nltech8 Threads: [ Previous | Next ]
Jay W

Posts: 35
Registered: 01/19/10
Looking for a 54845A service disk.
Posted: Jan 19, 2010 3:51 AM
Click to report abuse...   Click to reply to this thread Reply
Hello all,

I am looking for the 54845A service disk which is mentioned in the service manual and is part of the 54845-68803 service kit.
Specifically it is sub part 54810-68760 Infiniium Service Disk Pouch - I believe it's a floppy disk. Does anyone have a copy they'd be willing to email me?

Thanks very much for any help!

Jay
bans25

Posts: 4
Registered: 12/18/10
Re: Looking for a 54845A service disk.
Posted: Dec 18, 2010 2:11 PM   in response to: Jay W in response to: Jay W
Click to report abuse...   Click to reply to this thread Reply
I am looking to upgrade my scope to 4.5 but do not have a LS120 drive, were you able to do this?
bans25

Posts: 4
Registered: 12/18/10
Re: Looking for a 54845A service disk.
Posted: Apr 28, 2012 11:34 AM   in response to: bans25 in response to: bans25
Click to report abuse...   Click to reply to this thread Reply
Has anyone been able to upgrade to the latest software without a LS120 drive? I would like to get Web control of my scope
nltech8

Posts: 4
Registered: 08/13/10
Re: Looking for a 54845A service disk.
Posted: Apr 30, 2012 4:58 PM   in response to: bans25 in response to: bans25
Click to report abuse...   Click to reply to this thread Reply
If you are running a version older than 4.30 and want the webenable feature, you'll need to upgrade it to 4.30 before upgrading to 4.50. Also, if you're unit is really old and doesn't have much memory, you should stick to 3.72. That said, if you need to upgrade and don't have an LS-120 drive, there are others ways to do it. You need to get the files on to the hard drive some how. I've seen some 54845A's with a 2 USB port card installed. That would be the easist. An external parallel port CD-rom will work too if you happen to have one of those. Your other options involve removing the cabinet. You can either connect an internal CD-rom drive with an IDE cable to the PC mother board inside or you can remove the hard drive and connect it to a computer. I've done this with a $13 adapter cable that converts most internal hard drives to a USB drive. You need to copy the update/upgrade files to the 54845A's hard drive. The HP548UPG.ARQ and HP548UPG.HDR files need to be copied to the C:\scope\upgrade\scope\temp folder. The upgrade fold maybe be a hidden folder or it might not exist if you've never upgraded the firmware before. Create any folders necassary. The HP548LDR file goes in the C:\scope\bin folder. Now boot the unit up. After Windows finishes loading, you should get a white window telling you it's about to do a firmware upgrade. Just follow any directions. Sometimes when the unit reboots after the upgrade, it just powers off instead. Don't worry, just turn it back on.
nltech8

Posts: 4
Registered: 08/13/10
Re: Looking for a 54845A service disk.
Posted: Apr 30, 2012 5:03 PM   in response to: nltech8 in response to: nltech8
Click to report abuse...   Click to reply to this thread Reply
I just thought of another way to get the upgrade files copied on to your unit's hard drive. If you have a PC or laptop and a cross-over ethernet cable handy, you could setup networking between your 54845A and your PC.

Point your RSS reader here for a feed of the latest messages in all forums