Contact an Expert

Thread: Synchronizing 2 N6752A modules [N6700B]


Permlink Replies: 4 - Pages: 1 - Last Post: May 1, 2012 9:15 PM Last Post By: Joel Carlos Threads: [ Previous | Next ]
Joel Carlos

Posts: 3
Registered: 04/24/12
Synchronizing 2 N6752A modules [N6700B]
Posted: Apr 25, 2012 5:32 PM
Click to report abuse...   Click to reply to this thread Reply
Good day to all

I would like to ask an opinion if this kind of set-up is possible.

Hardware Set-up:
1 - Agilent N6700B Power supply mainframe.
2 - Agilent N6752A power supply module with High-speed test extensions.

Scenario:
- using the Listmode function provided by the High-speed Test extensions the 2 waveforms will be programmed on the Agilent N6752A power supply modules.

Problem for inquiry:

Synchronization
- to synchronize the execution of the 2 waveforms, I am planning to use the trigger out function of list mode on power supply module 1 to trigger the execution of power supply module 2. Is this possible on N6700B?
- If this is not possible, do you have any recommendation regarding this scenario?

Thank you very much to All!

Edited by: Joel Carlos on Apr 25, 2012 5:32 PM
MattC


Posts: 197
Registered: 03/19/10
Re: Synchronizing 2 N6752A modules [N6700B]
Posted: Apr 26, 2012 11:57 AM   in response to: Joel Carlos in response to: Joel Carlos
Click to report abuse...   Click to reply to this thread Reply
Hi Joel,

Yes there is a way to do this. You can use the following two commands:
LIST:TOUTput:BOSTep:DATA <Bool>{,<Bool>}, (@<chanlist>) - this command will generate a trigger at the beginning of the transient step.
LIST:TOUTput:EOSTep:DATA <Bool>{,<Bool>}, (@<chanlist>) - this command will generate a trigger at the end of each transient step.
You would need to set these up on the unit that you want controlling the timing.

On the unit that you want to trigger, you just need to set the transient trigger source to the transient on the first channel using:
TRIGger:TRANsient:SOURce TRANsient<n>, (@<chanlist>) where <n> is the channel you are triggering off of.

I think that this might be able to do what you are looking to do.

Note that the N6700B requires option 054 for this functionality.

Matt
Joel Carlos

Posts: 3
Registered: 04/24/12
Re: Synchronizing 2 N6752A modules [N6700B]
Posted: Apr 26, 2012 5:44 PM   in response to: MattC in response to: MattC
Click to report abuse...   Click to reply to this thread Reply
Hi Matt,

Thank you very much for the reply.

I would like to confirm that option "054" is "High Speed Test Extension".
Am i correct?

regards,

Joel Carlos
MattC


Posts: 197
Registered: 03/19/10
Re: Synchronizing 2 N6752A modules [N6700B]
Posted: Apr 27, 2012 3:02 PM   in response to: Joel Carlos in response to: Joel Carlos
Click to report abuse...   Click to reply to this thread Reply
Hi Joel,

Yes, option "054" is "High Speed Test Extension". I should have been clearer in my previous message.

Matt
Joel Carlos

Posts: 3
Registered: 04/24/12
Re: Synchronizing 2 N6752A modules [N6700B]
Posted: May 1, 2012 9:15 PM   in response to: MattC in response to: MattC
Click to report abuse...   Click to reply to this thread Reply
Thanks Matt

regards,

Joel

Point your RSS reader here for a feed of the latest messages in all forums