Contact an Expert

Thread: U2355A USB Visual C# Example


Permlink Replies: 4 - Pages: 1 - Last Post: May 17, 2013 10:46 AM Last Post By: BrianNorman Threads: [ Previous | Next ]
SteffenW

Posts: 1
Registered: 04/24/12
U2355A USB Visual C# Example
Posted: Apr 24, 2012 1:05 AM
Click to report abuse...   Click to reply to this thread Reply
Hello,

i'm looking for a simple c# example for the module U2355A to test the communication.
I want to install the "Agilent Modular Products Microsoft Visual Studio 2005 Project Templates" but the installation programm crashed allways. I use a Windows 7 system with the visual c# 2010 express developement software.
Can someone send me an example or a link.

Thanks very much.

Steffen
Mike

Posts: 65
Registered: 06/01/12
Re: U2355A USB Visual C# Example
Posted: Jun 1, 2012 7:44 AM   in response to: SteffenW in response to: SteffenW
Click to report abuse...   Click to reply to this thread Reply
Yes, I'd like to look at those too: also using VS 2010 and it raises error 1722 both on installation and uninstall.

Actually what I'm intending doing is communicating to a U2300 device from Java: I'm pretty familiar with bridging across to native code but I wanted to see the 'recommended' route e.g. using a .NET class that works directly with the module, via IVI, SCPI or the like through the Agilent I/O libs. Any pointers, code examples ( in C# would be okay ) most appreciated!

Mike Watts
hognala

Posts: 203
Registered: 04/09/07
Re: U2355A USB Visual C# Example
Posted: Jun 1, 2012 12:59 PM   in response to: Mike in response to: Mike
Click to report abuse...   Click to reply to this thread Reply
For the more general question, there should be some programming examples included with the IVI drivers for these devices. The IVI drivers can be downloaded from http://www.agilent.com/find/ivi

So Mike, you plan on using this Java code only on a Windows box? If on some other platform, what will you use as an I/O layer?

For LAN its pretty straightforward to use TCP/IP SOCKET's on port 5025, but there's not really a silver bullet for other interfaces, like USB, on non-Windows platforms.

Edited by: hognala on Jun 1, 2012 1:02 PM
Mike

Posts: 65
Registered: 06/01/12
Re: U2355A USB Visual C# Example
Posted: Jun 1, 2012 3:10 PM   in response to: hognala in response to: hognala
Click to report abuse...   Click to reply to this thread Reply
Thanks for that hognala. Yes, I found the IVI driver also includes lots of sample code,including for C# and works fine in VS 2010.

And yes, Java - it's a long history why it was used in the first place for this application - and it will only be on Windows. I might add the example to this as a thread when I get there as there is a fair interest in the subject in general. Whilst my choice would normally be VEE for test & measurement applications ( and indeed there is another app written in VEE which will be a snap to convert to use the U2352 ) but there are cases where Java might be a bettor choice - or like here where the choice has already been made.

Regards, Mike
BrianNorman

Posts: 2
Registered: 05/17/13
Re: U2355A USB Visual C# Example
Posted: May 17, 2013 10:46 AM   in response to: SteffenW in response to: SteffenW
Click to report abuse...   Click to reply to this thread Reply
Hi,

I am having the same trouble as the original post. I will be writing code in Visual C++ so the other suggestions don't help me. Windows 7, Visual Studio 2005.

Thanks

Point your RSS reader here for a feed of the latest messages in all forums