Contact an Expert

Discussion Forums are temporarily in read only mode. All forums are visible but posting is not possible. Please check back shortly.

Thread: Communication error while using RS-232 with BLDL SW.


Permlink Replies: 0 - Pages: 1
rakesh

Posts: 17
Registered: 04/20/12
Communication error while using RS-232 with BLDL SW.
Posted: Apr 20, 2012 1:58 AM
Click to report abuse...   Click to reply to this thread Reply
RS232 is not consider to be a very stable interface in order to communicate with the instruments.We always advise user to use either GPIB or LAN interface(in case of 34972/80) which is consider to be very stable interface.

Please find attached talking more about common RS232 problems.

Point your RSS reader here for a feed of the latest messages in all forums