Contact an Expert

Thread: requirements for print server?


Permlink Replies: 2 - Pages: 1 - Last Post: Mar 29, 2012 12:22 PM Last Post By: ksmith Threads: [ Previous | Next ]
aarons

Posts: 1
Registered: 01/09/12
requirements for print server?
Posted: Jan 9, 2012 12:36 PM
Click to report abuse...   Click to reply to this thread Reply
I just received a MSOX3014A, and am in the process of setting it up.

The network configuration is working (I can connect to the scopes web interface,) but I am unable to get a printer configured. I have a windows server 2008R2 print server, and I can print from other computers, but I constantly get the message from the scope that it failed to connect to the printer \\server\printername. I've tried using the raw ip of the server, fqdn, etc, but nothing works. Has anyone see this problem and solved it?

Thanks.

-Aaron
rainman50

Posts: 2
Registered: 01/11/12
Re: requirements for print server?
Posted: Mar 27, 2012 5:25 AM   in response to: aarons in response to: aarons
Click to report abuse...   Click to reply to this thread Reply
I have the same problem. We have 2 DSO X 3024A and we can't get either one to print at work. It comes up with failed configuration . We tried everything we could think of but still cannot get it to setup configuration to pass.

We gave up on printing from the instrument and just use the network browser method to print a screen shot.
ksmith

Posts: 130
Registered: 08/06/09
Re: requirements for print server?
Posted: Mar 29, 2012 12:22 PM   in response to: aarons in response to: aarons
Click to report abuse...   Click to reply to this thread Reply
network priniting was significantly imrpoved int he 2.10 release.

update the scope sw....

Point your RSS reader here for a feed of the latest messages in all forums