Contact an Expert

Thread: 86100D Trigger


Permlink Replies: 5 - Pages: 1 - Last Post: Apr 2, 2012 2:38 AM Last Post By: motoman89
motoman89

Posts: 14
Registered: 07/11/11
86100D Trigger
Posted: Mar 29, 2012 6:30 AM
Click to report abuse...   Click to reply to this thread Reply
Hello!
We bought an oscilloscope. At the stage set-up revealed a problem with the time base. The oscilloscope detects the amplitude of the signal amplitude characteristics can be measured, but the signal is displayed as a continuous band on the screen. The oscilloscope does not react to changes in the time base. How to achieve the normal form of the displayed signal? It is necessary to collect a special scheme of measurements using a trigger connector on the front panel or not? Go to the oscilloscope module has also been raised 86107A precision timebase, but it is not yet installed in the base module. Is it possible to work without the oscilloscope module, or it is required? What should be the circuit connecting it?
Thank You!
ksmith

Posts: 132
Registered: 08/06/09
Re: 86100D Trigger
Posted: Mar 29, 2012 12:21 PM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
te 86107A is not needed, but it will improve teh tiembase accuracy if used (correctly).

you need to feed the scope a clock at the front panel trigegr input. Which trigger option the scope has will determine what the max clock rate can be. check out the trigger section in the GUI...
jvo

Posts: 2
Registered: 02/23/07
Re: 86100D Trigger
Posted: Mar 29, 2012 12:31 PM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Hello,

It seems like your oscilloscope does not get the right trigger signal, or it is not setup to trigger on the signal it gets. In order to truly troubleshoot I'd need more information. This said here are a couple of hints:

  • It seems like you connected the signal to a measurement channel (i.e., a module in the mainframe)
  • Do you have a trigger signal connected to the trigger input at the front panel (such as a clock that is synchronous to your signal, or a pulse indicating when the signal repeats)?
  • Is the scope in free run mode or triggered on the front panel?
  • Is the signal repeating? All sampling scopes need a repeating signal/pattern except when in eye mask mode.
  • Press DEFAULT SETUP.
  • If your signal is not connected to channel 1 then turn off channel one and turn on the channel that your signal is connected to.
  • Then press AUTO SCALE
  • How fast is your signal or clock? You may have to change the trigger setup from "DC-3.2 GHz) to "Divided (13 GHz)"

My colleagues and I will be more than happy to further help you with the details. Feel free to send me a private message and I can help you further.

Best regards,

Joachim Vobis
Sales Development - Sampling Scopes
Santa Rosa, California

Edited by: jvo on Mar 29, 2012 11:43 AM
motoman89

Posts: 14
Registered: 07/11/11
Re: 86100D Trigger
Posted: Mar 29, 2012 10:48 PM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Hello!
Analog sine wave signal is fed from the output of the generator PSG 8257D to channel 1 of the oscilloscope directly. We tried to signal with varying frequency from 3 GHz to 40 GHz, but at any rate there is the timebase problem. Trigger connector on the front panel is not used. In the setting of the oscilloscope is set to free runes.
Thanks for information.
ksmith

Posts: 132
Registered: 08/06/09
Re: 86100D Trigger
Posted: Mar 30, 2012 11:50 AM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Right, you MUST have a trigegr signal at the front panel inout, and it MUST be synchronous with the signal going into CH1. The trigger signal cannot exceed 3 or ~12 GHz, depending on which trigger option you have.

feel free to call:

800 829 4444
motoman89

Posts: 14
Registered: 07/11/11
Re: 86100D Trigger
Posted: Apr 2, 2012 2:38 AM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Thanks for information.
Can we give the signal frequency of 40 GHz, the input module 86116C, or should we use the frequency divider?

Point your RSS reader here for a feed of the latest messages in all forums