Contact an Expert

 
User Profile
micahcruz
  Bronze
 
Name: micahcruz  
Status Level: Bronze (6)
Registered: Feb 9, 2012
Total Posts: 6
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: HP 54845 A with bad acqusition assembly.
 
I know it sounds crazy but just try to reload/reinstall the firmware for the scope. I have had many...
Re: 54845A Calibration Trigger Falure
 
I have seen these series of scopes do the same thing, pass all cal routines except for failing all t...
Re: HP54501A Calibration
 
The problem is with the on board "top Hat" battery installed on top of the NVRAM chip is dead. It ...
Re: HP 6030A again
 
when the overrange light comes on when trying to adjust output voltage above 0v that usually indiact...
Agilent 6038A Power Supply
 
I have 5 different 6038A power supplies that all do the same thing so I am pretty sure there is noth...
Re: 54835A self calibration error
 
I had the same exact problem with my 54835A that would fail the trigger portion of the self cal rout...