Contact an Expert

 
User Profile
CODER
  Bronze
 
Name: CODER  
Status Level: Bronze (11)
Registered: Feb 1, 2012
Total Posts: 11
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Agilent 3458A DMM waveform capture problem
 
Still need help with this. Any takers?
Re: Agilent 3458A DMM waveform capture problem
 
Thank you! I'll take all the help I can get.
Agilent 3458A DMM waveform capture problem
 
I’m trying to use the 3458A to do a real-time capture of the data comprising a periodic ramp that go...
"option not installed"
 
I'm programming an N6701 to output a voltage, then measure its current. It does so successfully but ...
cw stepped power sweep requirement
 
At a given CW freq, I need to step through input power levels (or do a binary search) through roughl...
Re: N52301A Pass/Fail
 
MUST it be calc:par:sel ? Can't one achieve the same with calc:par:def ?
creating a marker on N5230A
 
I'm trying to programmatically create a marker using the Labview driver shown on attached screenshot...
Re: Reading Marker info on N5230A
 
Thanks for the help. I tried that, selecting the trace, but it didn't help. Not sure what version in...
Reading Marker info on N5230A
 
I'm new to using this PNA, and experimenting slowly, one step at a time to understand its function a...
Re: Programming N6701 MPS
 
My mistake. Problem solved. I had the front panel meter in the wrong mode.