Contact an Expert

 
User Profile
Sparky
  Bronze
 
Name: Sparky  
Status Level: Bronze (9)
Registered: Jan 27, 2012
Total Posts: 9
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: What format is the number returned for :INPut:RECord:PLAY:POSition?
 
Thanks Dave, that's a lot more straight forward than plopping down markers...
Re: What format is the number returned for :INPut:RECord:PLAY:POSition?
 
This may be all moot, what I'm really tying to do is dynamically set overlap delay during a walk thr...
Re: What format is the number returned for :INPut:RECord:PLAY:POSition?
 
That will be very cumbersome to do in a test script its really to-bad there's now way to pull down t...
Re: What format is the number returned for :INPut:RECord:PLAY:POSition?
 
That helps, but I cannot reconcile the first number reported with what is displayed on screen 49481...
What format is the number returned for :INPut:RECord:PLAY:POSition?
 
Right now I'm having a problem trying to walk through a recording playback when the overlap has to b...
Re: 89601B VSA Not responding to SCPI Commands
 
High I just saw your request, I was logging into check on another new issue. I'm not sure if you wi...
Bug in 86901B SCPI interface when Triggering a Record on IF Magnitude.
 
As stated I have some inconsistency in using the SCPI interface. I had to change my working scripts...
Re: 89601B VSA Not responding to SCPI Commands
 
I did figure out what was going on: When sending VSA start command the application would launch but ...
Re: 89601B VSA Not responding to SCPI Commands
 
Is there a known issue with the Translator Framework and 89601B version 14.xx on XSA's using firmwar...