Contact an Expert

 
User Profile
odanzy
  Keysight Users
 
Name: odanzy  
Status Level: Keysight Users (1,543)
Registered: Nov 16, 2005
Total Posts: 1,543
City Columbia, Maryland
Country United States
Occupation Application Engineer
Website (example http://www.yoursite.com) http://www.agilent.com
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Too much data error when using the SCPI command MMEM:TRAN on the N5244A
 
I tried using the code I attached to transfer multiple SnP files (from 2 to 12 ports and a few kB to...
Re: Too much data error when using the SCPI command MMEM:TRAN on the N5244A
 
Take a look at the attached VI. I'm not going to say it is the cleanest, but it works and is pretty...
Re: Too much data error when using the SCPI command MMEM:TRAN on the N5244A
 
If this was just to change the name, then you could use MMEM:COPY instead and save quite a bit of co...
Re: Agilent 8714ES driver for LABView
 
There is an existing VXI Plug and Play Driver for the 8714 analyzer. That driver can be used in Lab...
Re: Too much data error when using the SCPI command MMEM:TRAN on the N5244A
 
How big of a file are you trying to transfer back to the PNA? I've successfully done around 1MB but...
Re: PNA-X 835 Series. How to use external input BNC1?
 
Are you looking to tell when the PNA receives a trigger on BNC1 and then wait for the measurement to...
Re: Measurements available with IVI driver
 
The measurement applications are not available in the IVI driver. I recommend taking a look at Agil...
Re: Applying a different calibration to DUT in PLTS after measurement
 
Michael, It isn't possible to apply the correction after the fact in PLTS. You could calibrate to ...
Re: How to save .s2p file in PC instead of saving in PNA itself?
 
The code attached may help.
Re: Using an 8753ES with PLTS 2012
 
PLTS 2012 doesn't support the 8753. Even older versions only supported the 8753 when used with an e...