Contact an Expert

 
User Profile
chard
  Silver
 
Name: chard  
Status Level: Silver (35)
Registered: Jul 24, 2007
Total Posts: 35
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: 3.5mm Male Open connector inside pin
 
For the PNA, the sex refers to the sex of the DUT or calibration standard. Male Open means the stan...
Re: Two Port VNA Measurement Setup
 
So, precision, low vswr attenuators placed adjacent to the DUT's input and output doesn't help, righ...
Re: Two Port VNA Measurement Setup
 
The connectors are both the same on the DUT. I'm using the unknown thru calibration technique.
Two Port VNA Measurement Setup
 
I'm measuring a passive two port network using an E5071B and performing a SOLT calibration with an 8...
Re: E4991A
 
Thanks for taking the time for this detailed response.
E4991A
 
Hello, I'm GPIB programming the E4991A impedance analyzer. I want to read the trace data from the a...
Re: VNA Measurement Uncertainty
 
measurement of esr of capacitors is not trivial.[/quote]What instrument and/or method is the most ac...
VNA Measurement Uncertainty
 
Hello, I downloaded the VNA uncertainty measurement calculator at http://www.agilent.com/metrology/...
N to SMA cable measurement
 
I've got a cable with an N connector on one end and an SMA on the other. I want to measure the cable...
Re: Simulate directional coupler based on measured data
 
Why can't you use an SnP component under "Data Items"? For a single directional coupler, you could u...