Contact an Expert

 
User Profile
motoman89
  Bronze
 
Name: motoman89  
Status Level: Bronze (14)
Registered: Jul 11, 2011
Total Posts: 14
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Measurements of planar capacitor characteristics
 
Hello! We are faced with the problem of distortion of a meander in the input circuit of the DUT. Pre...
E4980A LCR Meter
 
Hello! We purchased E4980A LCR meter. When measuring the impedance and phase shift at frequencies fr...
Re: 86100D Trigger
 
Thanks for information. Can we give the signal frequency of 40 GHz, the input module 86116C, or shou...
Re: 86100D Trigger
 
Hello! Analog sine wave signal is fed from the output of the generator PSG 8257D to channel 1 of the...
86100D Trigger
 
Hello! We bought an oscilloscope. At the stage set-up revealed a problem with the time base. The osc...
Re: LCA N4373C
 
Thank you!
LCA N4373C
 
Hello! I would like to clarify the following situation:The analyzer of optical components N4373 cons...
PSG E8257D
 
Hello! We plan to purchase an analog generator PSG E8257D. I would like to clarify: What is the maxi...
Re: Measurement of electro-optical parameters
 
Hello! Let me remind you, we need to measure the parameters of eye diagram of an integrated optical ...
Microwave Amplifier
 
Hello! I am interested in the following question: At the moment there is a microwave amplifier with ...