Contact an Expert

 
User Profile
raymond_shen
  Keysight Users
 
Name: raymond_shen  
Status Level: Keysight Users (8)
Registered: Jun 1, 2011
Total Posts: 8
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Reduce EMI with Shielded LAN Cables
 
Clip on RF chokes are less effective. We ran an experiment and applied a 10mm RF choke at the RF se...
Reduce EMI with Shielded LAN Cables
 
Unshielded LAN cables are often a source of unintentional RF emissions. These emissions may arise f...
How many sensors do you need?
 
Many people will ask "how many sensors will I need?" The answer, as I've said before, is an unsatis...
Geolocation accuracy
 
Many people ask us what is the accuracy of the geolocation system? The answer is an unsatisfying it...
SAL API Demo code
 
C# code for demo applications using the SAL API are installed on your computer together with the sen...
Signal Surveyor N6820E
 
RF Sensor users may or may not need Signal Surveyor. Signal Surveyor provides a means of triggering...
Indoor geolocation
 
The sensors can also be used for indoor geolocation as well as outdoor geolocation. A tip is to us...
New blog for over-the-air RF Sensors
 
Agilent has just released a new blog for over-the-air interface RF Sensors, which is Agilent N6841A....