Contact an Expert

 
User Profile
brian@boeing
  Silver
 
Name: brian@boeing  
Status Level: Silver (17)
Registered: Jun 1, 2011
Total Posts: 17
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Updating imported .NET library
 
I guess what would be handy is a way to refresh the imported DLL in a quick operation versus closing...
Updating imported .NET library
 
.NET Assembly References it copied the DLL file to the working directory of the VEE project. Right n...
E4440A measurement completion time
 
We're programming the E4440A remotely via a C++ device handler. One of the requirements is to provid...
Re: 3458A keypress SRQ
 
Ok, I'll look at that. I suspect we will end up telling them that they can't do that. Thanks,Brian
3458A keypress SRQ
 
We normally operate the unit remotely. We're looking into a request to be able to have the operator ...
3458A ACV overload
 
I'm setting up and taking various measurements remotely. One thing that has me puzzled is the AC V m...
Re: N9030A setup instruction
 
Ok, that sounds great. I thought we were good, that confirms it. Thanks for the information. Brian
N9030A setup instruction
 
I am programming the instrument remotely, using a C++ program. Currently, I only use *OPC during mea...
Re: 3458A self-test
 
Thank you.Brian
Re: 3458A self-test
 
Ah, ok. Thanks.Brian