Contact an Expert

 
User Profile
golfnut
  Bronze
 
Name: golfnut  
Status Level: Bronze (13)
Registered: Mar 7, 2011
Total Posts: 13
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: FIFO buffer data order
 
My apologies for my lack of clarity. Let me try to explain. I mentioned emphasizing the FIFO Sweep...
Re: FIFO buffer data order
 
I looked at the help page you linked. As a user who is primarily focused on antenna measurements, I...
FIFO buffer data order
 
Does anyone have the full data order for the FIFO buffer on a two port PNA-X? The help file doesn't...
Re: PNA, DCOM, and SourcePowerCalibrator Object : AcquirePowerReadingsEx error
 
Thanks for the help on that issue. I never would have figured that out. I assumed that the source ...
PNA, DCOM, and SourcePowerCalibrator Object : AcquirePowerReadingsEx error
 
I'm trying to perform a source power calibration with a power meter by issuing the DCOM commands fro...
Re: PNA, DCOM, & Matlab: meas.PutDataComplex
 
That worked. For reference the following script works, but I do have to create a 21x2 array: x=(1:...
Re: PNA, DCOM, & Matlab: meas.PutDataComplex
 
Sadly, that doesn't solve the problem. I imagine something in the pnaproxy.exe setup defines the st...
PNA, DCOM, & Matlab: meas.PutDataComplex
 
Does anyone have an example script for uploading data into a PNA from Matlab on a remote PC via DCOM...
PNA 8362B
 
Does the 8362B PNA allow for segment frequency sweeps from high to low? That is, can it start at th...
Re: 64-bit pnaproxy.exe
 
I eagerly await its arrival!