Contact an Expert

 
User Profile
LOlson
  Silver
 
Name: LOlson  
Status Level: Silver (21)
Registered: May 21, 2007
Total Posts: 21
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: PSA Preselect Center Errors
 
Thanks, I did some research on YIG filters and understand now the issue with the preselector centeri...
PSA Preselect Center Errors
 
We recently started using the preselector center function of E4448A as we found that the YTF input f...
Re: VMC measurements of a two stage downconverter in fixed IF mode
 
Dr. Joel, The DUT has 2 LO external inputs. For verifying I could make a valid cal and measurement, ...
VMC measurements of a two stage downconverter in fixed IF mode
 
I have been running through the setups for measuring a two mixer downconverter. I have managed to do...
PNA E8364B source power CAL via GPIB
 
If you mean that you have your computer connected to the PNA with the USB to GPIB interface connecte...
LO Name Selection
 
Just a quick note that the LO name selection appears to be buggy manually or by remote command. In t...
External Source Connection Prompt
 
I am using SCPI commands with LabWindows/CVI. I anticipated your response and added a prompt after I...
Source Power Cal
 
I looked at the example yesterday morning and our SMC mixer calibration code and realized that we we...
Thanks
 
Thanks,I'll try it in the morning. It looks like it is just what I needed. It is strange that the he...
Remote Selection of an External Source
 
I called the support line and received a case ID but no one was available at the time and I need a r...