Contact an Expert

 
User Profile
John Miles
  Gold
 
Name: John Miles  
Status Level: Gold (72)
Registered: Jan 30, 2006
Total Posts: 72
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Full 2-Port vs. Economy VNAs
 
If you want to characterize a two-port nonreciprocal device -- say, an amplifier -- it's a pain in t...
Re: Why are Agilent scopes not able to measure in the sample memory?
 
Also worth noting that the ability to make record-based measurements was just added as an option ...
Re: MSO6000 series issue: Channels suddenly switch to 50Ohm
 
Starting to see it happen here as well (MSO6054A MY44002353). Not common enough yet to be a real nu...
Re: Noise spectrum measurement via remote control
 
You can use the 85671A noise measurement module (sometimes available on eBay, but no longer sold by ...
Re: 34461A Front Panel Power Lamp (two colors)
 
Agreed that the 34461A is best left powered on, if only because the bootup time is longer than most ...
Re: DSOX3024 HV DC Offset
 
Wow, good catch. I've never heard of scope damage caused by using a HV probe in AC-coupled mode, bu...
Re: 8562e hangs the GPIB bus from cold power up
 
ID? will return the ID string on an 8560E-era instrument. If you do need to clear the analyzer's G...
Re: How to do correlation with the 35670A?
 
The feature you're looking for is probably labeled "Cross spectrum." In combination with display av...
Re: dbm measurement.
 
Agreed, this would be nice to have. If you can show RMS voltage, which you can, and if you can sele...
Re: Measurement Uncertainty for 53230A
 
IANAAE (I Am Not an Agilent Employee), but just to give you some insight into their likely thought p...