Contact an Expert

 
User Profile
aus10
  Bronze
 
Name: aus10  
Status Level: Bronze (6)
Registered: Apr 29, 2010
Total Posts: 6
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: PNA-X SCPI Command to Enable LO1 Calibration in SMC Guid
 
Thanks for the speedy response! Can always count on Joel, Dara, and friends to get you answers here!
PNA-X SCPI Command to Enable LO1 Calibration in SMC Guided
 
I'm trying to do a remotely commanded SMC guided cal with an ECAL and I want to add the "Additional ...
PNA-X SMC with Phase Remote Programming
 
I am trying to do a SMC cal with phase remotely and have found that my phase measurement is erroneou...
Re: PNA-X Labview Driver
 
Yes, I've observed that most vi's work individually. However, It seems like there a quite a few vi'...
PNA-X Labview Driver
 
I'm having some problems with the Labview 8.5 Driver (11/2009) that I downloaded from the following ...
PNA-X Beta Firmware
 
I noticed that there is a new beta firmware for the PNA-X (PNA_A092002.msi). Are there any release ...