Contact an Expert

 
User Profile
janvh
  Keysight Users
 
Name: janvh  
Status Level: Keysight Users (37)
Registered: Jun 8, 2009
Total Posts: 37
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: python excetion in FEM simulation EMPRO2013_07
 
Hello Davide, The error is not specific enough to diagnose the problem. Can you contact your local...
Re: Stripline simulation using FEM
 
Hi, The problem seems to be related to the port definition, so you can try the following: re-enter ...
Re: FEM electromagnetic Simulation: consistency and convergence issues
 
Thank you for your feedback. We have conducted specific tests to reproduce the problem you indicated...
Re: Text Not Showing Properly
 
Options ... General tab |Can you describe the hardware and OS you are using?
Re: importing virtual family human model in raw(voxel) format
 
EMPro supports the .mmf file to import Voxel objects. The best path is to find a way to convert the ...
Re: Python Scripting
 
Work is planned to expand the Python Scriptin documentation beyond what is currentlyu available in t...
Re: Meshing
 
This primarely depends on the complexity of the antenna or object, its electrical size and the compu...
Re: How to contact a silicon substrate?
 
It is possible to model substrate contacts with Momentum. To do this, use the following substrate de...
Re: Editing designkits in Advanced Model Composer
 
You are correct if you only use parameters with contiuous ranges. For these, you can delete the .rat...
Re: tunning input port impedance
 
You can use layout components if you have multi-layer design. Just setup the design for multi-layer ...