Contact an Expert

 
User Profile
cainelee
  Bronze
 
Name: cainelee  
Status Level: Bronze (5)
Registered: Jun 8, 2009
Total Posts: 5
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Create folder
 
I would like to ask if there is any built-in function or statement in ICCAP which could create a fol...
one-port S-parameter converting tow-port
 
hello, Is there any built-in function or equation in ADSwhich could convert the one-port S-parameter...
How to calculate mean value ??
 
Hello  I would like to ask how do I calculate mean value from a set of nmber? I find a built-in...
Re: Access value of specified variable
 
Thanks for your support~.It's really helpful.
Access value of specified variable
 
Hello I'm a new guy in using ICCAP. The version of software is 2004. If there is any command bult-in...