Contact an Expert

 
User Profile
zubair_rafiq
  Bronze
 
Name: zubair_rafiq  
Status Level: Bronze (11)
Registered: May 29, 2009
Total Posts: 11
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: N5224 Vs E8363B
 
I do not want any remote mixing or H11 option. I think only N51224-201 will work for me. please guid...
N5224 Vs E8363B
 
I am intended to buy N5224A-201 or N 5244A for Antenna Measurement in chamber w/o remote mixing. the...
E8363B Mixer Source unleveled PL Lost at same time
 
SC21 then PNA immediately shows message source unleveled at the same time Phase lock lost . I set mi...
Re: E8363B Mixer /Freq. Offset test Problem
 
Oops, last year it has been discussed in detail with Daniel Yap, Mr John V about A07.50xx and we cou...
E8363B Mixer /Freq. Offset test Problem
 
I have E8362B with 080,081,083,014,UNL,H11 etc. also 83631B Signal generator. I don’t have any refe...
Power Sweep Range E8362B
 
I am using E8362B with all options except noise figure options. i read help file unfortunately , i a...
Re: how to test the S11, S12, S21, S22 of my LNA demo board
 
Agilent’s Expert can explain this much better however, I believe that following may be useful after ...
Noise figure measurement with Freq. Offset Options E8362B
 
I have Freq. Offset Options e.g 081, 080, H11 etc so i cannot get noise figure measurement option in...
Re: setting, reading marker value remotely over GPIB using Matlab?? E8362B
 
“CALC:MARK:Y?” may be help you. Before this you may set something like “CALC:MARK:X 2e9” Here % NA ...
E8363B recieved value higher than expected
 
Dear All I have installed PNA in atteched configuration. Sometimes value of CH B/A is 5dB apprx. hig...