Contact an Expert

 
User Profile
t_stinchcombe
  Silver
 
Name: t_stinchcombe  
Status Level: Silver (29)
Registered: Jul 14, 2008
Total Posts: 29
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: How to ignore 'bad cylinder groups' on disk - SOLVED, ma
 
We think we may have gotten around this problem, without having to do a full system build (as severa...
How to ignore 'bad cylinder groups' on disk - SOLVED
 
This is really a HPUX question, so if anyone can point me to a better forum in which which to post t...
Re: Need LabVIEW VIs for Agilent 4156C SMU
 
As interesting as your problem sounds, I think it unlikely that you will get much response here, as ...
Share your tips on how to keep personality pins clean
 
Hi list, Of necessity our 3070s are used in an environment which includes our cardboard packing boxe...
Re: Capacitance measurement method and accuracy
 
A variety of circumstances has caused me to return to the original problem that made me start this t...
Re: Crystal Measurement
 
Hi Simon, "We are experiancing problems, trying to measure a 20MHz Crystal connected to a Renesas H8...
Re: Missing 'fetch' syntax, and undocumented 'measure' feature?
 
Hi Calvin, "Useful info here on the "fetch (analog)" syntax and usage from my notes from the User Fu...
Missing 'fetch' syntax, and undocumented 'measure' feature?
 
This post is in two parts: I'll deal with the trivial first. We are using Unix controllers (B180L), ...
Re: measuring capacitors in powered mode
 
Hi Marco, I have no direct experience of trying this, and when I first saw it a few days ago my imme...
Re: Battery measure
 
This one is easy, as I've had a copy for ages (it is useful) "and also about the workings of dischar...