Contact an Expert

 
User Profile
Suchita
  Bronze
 
Name: Suchita  
Status Level: Bronze (4)
Registered: May 14, 2012
Total Posts: 4
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Re: Capture Demodulated IQ samples
 
I am aware of that. I captured IQ Meas Time samples at both 1 Point/symbol and at 4 Point/symbol. 1s...
Re: Capture Demodulated IQ samples
 
If I plot the constellation generated by IQ Meas Time captured data, I see them to be all over the p...
Re: Capture Demodulated IQ samples
 
I would like to capture the IQ samples after demodulation but before they are converted in the symbo...
Capture Demodulated IQ samples
 
Is there a way to capture the demodulated IQ samples. I had captured IQ MeasTime trace earlier but a...