Contact an Expert

 
User Profile
Steve Reeves
  Silver
 
Name: Steve Reeves  
Status Level: Silver (25)
Registered: Mar 6, 2008
Total Posts: 25
   


Recent Messages: Point your RSS reader here for a feed of the latest messages in all forums
Spectrum Analyzers - Why use Min Hold trace detector
 
I notice that many of the Agilent (HP, Keysight) spectrum analyzer models have a Max Hold and Min Ho...
CPU fan for 8753E 8753ES network analyzers
 
Anyone know of a good replacement for the CPU fan part # 5060-8776 used on the CPU for the 8753E, 87...
Re: N9030A PXA - absolute amplitude amost 2 dB high
 
From what you describe, this sounds like it MAY be a case of the 50 MHz internal calibrator circuit ...
N9030A PXA - absolute amplitude amost 2 dB high
 
I am looking at an Agilent N9030A PXA that's coming up for its first year cal. The Absolute Amplitud...
Can I get F/W upgrade for N9020A (MXA) prior to A.10.05 ? This one failed.
 
Hi. I recently attempted a firmware upgrade on a problem N9020A (F/W ver. A.01.44). Following the i...
Re: How to remove 8156A front panel bezel?
 
Mike, Thanks ! That was all I needed - it was a very smooth removal process.Steve
How to remove 8156A front panel bezel?
 
Hi. I have an 8156A that appears to have a dead display module - fan runs and I hear the shutter tur...
Re: E5071C RF Power output accuracy
 
Thanks for the reply, but what I'm looking for is not the output power range of the E5071C, but rath...
E5071C RF Power output accuracy
 
Does anyone know if the E5071C adjustment software is capable of raising the RF Output Power enough...
E4443A PSA Auto-Align stability
 
What range of stability should the PSA series show during cycle-to-cycle run of the Auto-Align proce...