Contact an Expert

Thread: 53132 return multiple results


Permlink Replies: 0 - Pages: 1
dewaynecurry

Posts: 1
Registered: 10/05/11
53132 return multiple results
Posted: Oct 6, 2011 7:48 AM
Click to report abuse...   Click to reply to this thread Reply
I am trying to update a code base that used a Fluke PM6880B to gather multiple totalize results and return them in an array. Is there a way to do so with the Agilent 53132A Counter? Herte is the original code I am translating for reference:
// ' UUT outputs bursts of pulses; number of pulses in each burst = test code just
// ' executed. Pulses are 300 nS per cycle; 2 - 4 mS between bursts. Counter is
// ' setting internal gate window of 1 mS and measuring bursts repeatedly, putting
// ' results into array. ITA includes resistive 10x divider on pulses.
// Call subvsr("Counter,{:CONF:TOTALIZE:TIMED 1e-3,(@1),(@1)},##")
// Call subvsr("Counter,{:INP:SLOPE NEG},##")
// Call subvsr("Counter,{:INP:COUP DC;:INP:LEV 0.3;:INP:LEV:AUTO OFF},##")
// Call subvsr("Counter,{:INIT:CONT ON},##")
// Call subvsr("DIO,Reset Bit,APB6,##") 'Set Factory Test bit LO; holds any failed test
// Call ApplyPower
// Call subvsr("Delay,7,##")
// Gpib_OUTPUT "Counter", "FETCH:ARRAY? -1"

Point your RSS reader here for a feed of the latest messages in all forums