Contact an Expert

Thread: Switchin Front/Rear Terminal on 34401


Permlink Replies: 2 - Pages: 1 - Last Post: Jan 16, 2012 2:14 AM Last Post By: rossano
rossano

Posts: 2
Registered: 01/13/12
Switchin Front/Rear Terminal on 34401
Posted: Jan 13, 2012 10:10 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I would like to know if it is possible, on 34401, to automatically switch between front terminal and rear terminal passing a GPIB command.
On the 34401 manual I only found this GPIB command:
ROUTe:TERMinals?

which reports which one is active but does not allow to set it!

Does anyone know if it is possible to do it?

Thanks a lot for any help
Rossano
lhornburg

Posts: 492
Registered: 01/15/10
Re: Switchin Front/Rear Terminal on 34401
Posted: Jan 13, 2012 10:26 AM   in response to: rossano in response to: rossano
Click to report abuse...   Click to reply to this thread Reply
Sorry no, there is not a command to do this. It is a physical switch that must manually be pressed to switch from front to rear and vice versa.
rossano

Posts: 2
Registered: 01/13/12
Re: Switchin Front/Rear Terminal on 34401
Posted: Jan 16, 2012 2:14 AM   in response to: rossano in response to: rossano
Click to report abuse...   Click to reply to this thread Reply
Thanks a lot for the prompt reply!

Although it is a pity that it is not possible to set the input terminals remotely (it obliges me to use two multimeters) your quick answer has saved quite a lot of time !

Thanks
Rossano

Point your RSS reader here for a feed of the latest messages in all forums