Contact an Expert

Thread: E4418B RF Pwr Meter firmware update problem


Permlink Replies: 7 - Pages: 1 - Last Post: Sep 10, 2010 1:45 PM Last Post By: Desertcatfish
Desertcatfish

Posts: 10
Registered: 09/03/10
E4418B RF Pwr Meter firmware update problem
Posted: Sep 3, 2010 3:29 PM
Click to report abuse...   Click to reply to this thread Reply
So my "new guys" fried two of my old power sensors... Company purchased Agilent N8481A Pwr Sensors($1200 ea), which should work with our power meter E4418B. I need to update my firmware to latest version for them to work, already upgraded the DSP board ($523), so here is the problem-

Even though the E4418B has an RS-232 (we don't use GPIB at all) connector on back; there is no menu selection to choose it over GPIB, even though the manual says there is. I don't want to spend more on a GPIB PCI board and cable just for a simple firmware update.

Firmware installed is A1.03.00 and I need the latest one A1.09.01

The manual says under menus = System/Input -> Remote Interface -> Select Interface, should let me choose between HPIB or Serial. My E4418B instead of displaying Remote Interface shows HPIB.


Any ideas or help would be appreciated
Desertcatfish

Posts: 10
Registered: 09/03/10
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 3, 2010 6:27 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
Why are posts concerning RF power meters in the Power supplies section? A RF power meter has nothing to do with AC or DC power supplies. Where I posted earlier is where power meter posts should go. Maybe I misunderstand?
jvall

Posts: 528
Registered: 12/08/05
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 3, 2010 8:44 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
I gotta say, it's hard to argue with your logic...this makes absolutely no sense at all. You did not misunderstand. I am not sure why this was moved here.
The guy that I was going to have answer your question will never find this post now.
I will try to remember to remind him, but that won't be until Tuesday.

Meanwhile try looking at these sites:
http://www.home.agilent.com/agilent/edi ... id=1377930

http://www.home.agilent.com/agilent/red ... .536881895
odanzy

Posts: 1,543
Registered: 11/16/05
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 5, 2010 5:47 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
I'm curious if you check the Version information System->(More)->(Service)->(Version), if the power meter thinks it is the E4418A instead of the B. Since you have changed the DSP board more than likely the memory was reset as would happen during the security/memory clearing process. Since the A model did not have a serial port, this would explain why none of the menu structures are present.

If this is the case, it is necessary to reload the information using SCPI commands using GPIB. The process is discussed at this link: http://www.home.agilent.com/agilent/edi ... SR.General
Desertcatfish

Posts: 10
Registered: 09/03/10
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 9, 2010 5:08 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
I don't have a GPIB interface board or cable, we don't use it. I guess I either need to send it in for the firmware update or purchase a GPIB board and cable. Is it possible to use the 82357B GPIB to USB adapter to do the firmware update? It would be much cheaper and easier for us to use.

-Thanks
odanzy

Posts: 1,543
Registered: 11/16/05
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 10, 2010 6:29 AM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
The 82357B USB-GPIB interface will work.
Desertcatfish

Posts: 10
Registered: 09/03/10
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 10, 2010 12:53 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
Ok thanks, see if I can sell this one to the govt. now...
Desertcatfish

Posts: 10
Registered: 09/03/10
Re: E4418B RF Pwr Meter firmware update problem
Posted: Sep 10, 2010 1:45 PM   in response to: Desertcatfish in response to: Desertcatfish
Click to report abuse...   Click to reply to this thread Reply
BTW yes the Power Meter shows model number as E4418A now...

Point your RSS reader here for a feed of the latest messages in all forums