Contact an Expert

Thread: HP8561A


Permlink Replies: 3 - Pages: 1 - Last Post: Mar 10, 2012 10:50 AM Last Post By: sm7ovk
ON4IMM Dirk

Posts: 9
Registered: 09/15/10
HP8561A
Posted: Oct 21, 2010 6:46 AM
Click to report abuse...   Click to reply to this thread Reply
Hello
I have a HP8561A work very well,thill a few day's ago the display is dead. I have this fault before but after swicth on/off the diplay whas OK, also the SA work very well.
I mesaure the cal output ,this signal is OK , The "video output " on the rear off the SA d'ont work ,i think it is a video failure
ANY have a link for a service manual ?? or a solution for this problem.

Tnx in advance

ON4IMM Dirk
tabbott


Posts: 1,483
Registered: 07/24/09
Re: HP8561A
Posted: May 4, 2011 9:12 AM   in response to: ON4IMM Dirk in response to: ON4IMM Dirk
Click to report abuse...   Click to reply to this thread Reply
Hi -

The VIDEO OUTPUT of the 8561A is not a composite video signal that can be applied to a video monitor. The Video Out is a buffered version of the output of the envelope detector, which comes immediately after the log amplifier. It is more suitable to be applied to a strip chart recorder, waveform recorder, or oscilloscope. You can use the Sweep Out to drive the horizontal axis of a ‘scope and the Video Out to drive the Y-axis.

However, bear in mind that the Video Out signal is not calibrated.

Regards -




Relevant Products:#8561A#
lanecalde

Posts: 1
Registered: 02/09/12
Re: HP8561A
Posted: Feb 9, 2012 11:26 PM   in response to: ON4IMM Dirk in response to: ON4IMM Dirk
Click to report abuse...   Click to reply to this thread Reply
Sorry for late reply...,Hope this link will help you..
http://tech.groups.yahoo.com/group/hp_a ... equipment/
sm7ovk

Posts: 53
Registered: 01/24/08
Re: HP8561A
Posted: Mar 10, 2012 10:50 AM   in response to: lanecalde in response to: lanecalde
Click to report abuse...   Click to reply to this thread Reply
Hi,

Have you opened the unit? Please note that there are high voltages present so please don't do this if you haven't the skills! The high voltages can kill!
When the unit is open there are a couple of LEDs indicating voltages - are all on?
Most probably some of the electrolytic capacitors in the monitor unit is bad. These tend to dry out and it's a very frequent error.
I'm not sure how your spectrum analyzer looks like but on my 8594E the monitor with its casing could be lifted out and I changed the faulty capacitors. You can find the faulty one if you very carefully heat them a little. When the monitor starts to work you have found the faulty one - BUT once again DO NOT try this if you haven't worked with high voltages before!
There are some spectrum analyzers with a "monitor output" on the rear, this can be connected to an external monitor.

Best Regards - 73
Jens

Point your RSS reader here for a feed of the latest messages in all forums