Contact an Expert

Thread: Replace CRT HP8591 seir


Permlink Replies: 2 - Pages: 1 - Last Post: Sep 22, 2010 4:39 AM Last Post By: ON4IMM Dirk
ON4IMM Dirk

Posts: 9
Registered: 09/15/10
Replace CRT HP8591 seir
Posted: Sep 19, 2010 9:50 AM
Click to report abuse...   Click to reply to this thread Reply
Hello
I have buy a lot off 2x HP8591A specrtumanalyzers_2xHP8591C Cable TV analyzers and 1 HP8591A. The CRT's from all that analyzers are pracitcal dead.Have 10 new CRT Omnivison LP0615E3Y and the replacement is no problem........but there are two analyzers with CRT Model TR- 60S1A from Matsushita (equal size and connectors) but the problem is that there is no Synchronisation . The screen give horizontale lines , ANY now what to do with these problem ??

Have 3 new CRT Omnivison LP0615E3Y in stock any need one PSE mail me

Thanks
Dirk
Belgium
Mike M


Posts: 268
Registered: 04/10/07
Re: Replace CRT HP8591 seir
Posted: Sep 20, 2010 3:35 PM   in response to: ON4IMM Dirk in response to: ON4IMM Dirk
Click to report abuse...   Click to reply to this thread Reply
The instruments that you have do not all have the same horizontal sync rates, and they used different monitors.

The 8591C has the same sync rate as the 8591E, which is 15.75 kHz, while the 8591As have a sync rate of 19.2 kHz. So you will need different monitors for each...

The OmniVision monitors you mention are the 15.75 kHz variety and were previously sold by Agilent as part of the 08590-60377 assembly for display replacement.
ON4IMM Dirk

Posts: 9
Registered: 09/15/10
Re: Replace CRT HP8591
Posted: Sep 22, 2010 4:39 AM   in response to: ON4IMM Dirk in response to: ON4IMM Dirk
Click to report abuse...   Click to reply to this thread Reply
Thank Mike for quick reply and info. Maby i cant rebuild the 8591A CRT chassis with the sync rate of 19.2 kHz by change the 'Cathode Ray Tube' and left the electronic boards.


Tnx again
Dirk

Point your RSS reader here for a feed of the latest messages in all forums