Contact an Expert

Thread: N4373A Lightwave Component Analyzer


Permlink Replies: 1 - Pages: 1 - Last Post: Mar 15, 2012 9:22 AM Last Post By: olfu
r7f8g71

Posts: 1
Registered: 07/03/07
N4373A Lightwave Component Analyzer
Posted: Jul 3, 2007 9:54 AM
Click to report abuse...   Click to reply to this thread Reply
Does anybody know if the 87075C can be used as a complement of the N4373A system? Is the operating or user manual for the N4373A available? Is the N4373A system available in 75 Ohms (N Type)?

Edited by: mkelly on Mar 15, 2012 9:22 AM
olfu

Posts: 13
Registered: 02/06/07
87075 with N4373A LCA
Posted: Jul 6, 2007 9:59 AM   in response to: r7f8g71 in response to: r7f8g71
Click to report abuse...   Click to reply to this thread Reply
We have made no tests with with N4373A and the 87075C, but
in principle this should work. I recommend to use the mechanical
switch version of the 87075C. However this configuration might
not meet the original specification of the N4373A system.

If you need a users guide you can ask your local Agilent sales representative. The Agilent number for this N4373-90A01.

The Agilent LCA N4373A is not available with 75Ohm, but with a
minimum loss pad you can adapt for 75Ohm. The N507X
Network analyzer offers a procedure to correct for the measurement errors.

Point your RSS reader here for a feed of the latest messages in all forums