Contact an Expert

Thread: VEE osciloscope aplication for DSO7000b


Permlink Replies: 1 - Pages: 1 - Last Post: Feb 13, 2012 6:42 AM Last Post By: bret
Kejklir

Posts: 1
Registered: 02/13/12
VEE osciloscope aplication for DSO7000b
Posted: Feb 13, 2012 5:27 AM
Click to report abuse...   Click to reply to this thread Reply
Hi, i need to retreive data from osciloscope DSO7000b series into vee program for next use (remote osciloscope and other). I wasnt able to find even some example of that. Is there some function which return data wiewed on screen of instrument? Or there are some examples which i missed?
bret

Posts: 89
Registered: 07/05/11
Re: VEE osciloscope aplication for DSO7000b
Posted: Feb 13, 2012 6:42 AM   in response to: Kejklir in response to: Kejklir
Click to report abuse...   Click to reply to this thread Reply
I'm not very familiar with VEE (only used it for 30 seconds), but at the SCPI level, the command to get screen-shots is :DISP:DATA? <args>. Set your VEE command setting to save the returned value as a file.

If it's waveform data that you want, :WAV:DATA? is the command.

Point your RSS reader here for a feed of the latest messages in all forums