Contact an Expert

Thread: N5230C Source Power Cal


Permlink Replies: 2 - Pages: 1 - Last Post: Feb 21, 2012 5:52 PM Last Post By: bhokkan
totalaj

Posts: 9
Registered: 04/18/06
N5230C Source Power Cal
Posted: Feb 21, 2012 9:14 AM
Click to report abuse...   Click to reply to this thread Reply
When performing a Source Power Calibration, can the power meter be on the same GPIB bus as the network analyzer, or does the power meter have to be connected to USB port on the network analyzer? Is there a way to configure so we can perform source power cals when needed, but not have to communicate with the power meter through the analyzer?

Hardware:
N5230C (Controlled by station PC over GPIB, LAN to network switch)
N1914A
E9300H

Thanks!
daras


Posts: 920
Registered: 12/01/05
Re: N5230C Source Power Cal
Posted: Feb 21, 2012 10:34 AM   in response to: totalaj in response to: totalaj
Click to report abuse...   Click to reply to this thread Reply
all of our C model PNAs have two GPIB ports on the back. One is marked "Controller", and the other is marked "Talker/Listener". whenever, the PNA is going to control an external GPIB device (ex. a power meter for source power cal), then that device should be connected to the GPIB port marked "Controller" or it can be connected to USB port via a USB-GPIB adapter. However, it should never be on the same bus as the PNA's Talker/Listener port.
bhokkan

Posts: 340
Registered: 12/01/05
Re: N5230C Source Power Cal
Posted: Feb 21, 2012 5:52 PM   in response to: totalaj in response to: totalaj
Click to report abuse...   Click to reply to this thread Reply
As Dara stated, you can connect your power meter to the PNA's GPIB Controller port or a USB-GPIB adapter. But as I see you mentioned your meter is a N1914A and those have a device-side USB control port, the PNA can control the meter just via USB if you wish. Once you make the USB connection, in the PNA's Power Meter Settings dialog you'd select 'USB' and the meter's ID should then be seen to be selectable there.

Point your RSS reader here for a feed of the latest messages in all forums