Contact an Expert

Thread: FieldFox 9912


Permlink Replies: 1 - Pages: 1 - Last Post: Feb 13, 2012 12:31 PM Last Post By: am95405
bferek

Posts: 1
Registered: 02/13/12
FieldFox 9912
Posted: Feb 13, 2012 3:14 AM
Click to report abuse...   Click to reply to this thread Reply
I have a specific application whereby a single frequency (20 MHz) S11 shoul be measured with sweep time of 20 seconds. How does the remote data acquisition function? Can I download the data while the sweep is running, or I can only download the data after the sweep has been stopped?
am95405


Posts: 210
Registered: 12/05/05
Re: FieldFox 9912
Posted: Feb 13, 2012 12:31 PM   in response to: bferek in response to: bferek
Click to report abuse...   Click to reply to this thread Reply
Hi,

"You can query the data before the sweep completes, but you have no idea how much (if any) of the returned data will reflect the results of the current sweep. For example:

INIT:IMM
CALC:DATA:FDATa?

Will likely return an array with some data from the just-started sweep, and some data from the last sweep. Using *OPC? or *WAI will fix this problem:

INIT:IMM
*WAI
CALC:DATA:FDATa?

All this is because INIT:IMM is defined as an 'overlapped' SCPI operation, meaning that the SCPI parser will continue parsing new commands while INIT:IMM is still running (those new operations are overlapped (in time) with the INIT:IMM operation)."

Regards,
Afsi

Point your RSS reader here for a feed of the latest messages in all forums