Contact an Expert

Thread: Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)


Permlink Replies: 3 - Pages: 1 - Last Post: Jul 16, 2012 4:20 PM Last Post By: DaveHornbeck
sartaj

Posts: 2
Registered: 07/06/12
Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)
Posted: Jul 6, 2012 3:56 AM
Click to report abuse...   Click to reply to this thread Reply
I need to know what all parameters need to be set for a clustered sc-fdma measurement for LTE-Advanced FDD. The resource allocator used for LTE-Advanced is the same as LTE and does not contain anything specific to setting up the two clusters for each slot. The auto-mode fails to syn when a LTE-Advanced signal is feeded in to the analyser. the help says that it is capable of demodulation clustered SC-FDMA. Also, does the size of the two clusters need to be same in each slot (number of resource blocks allocated be same)?
DaveHornbeck

Posts: 65
Registered: 03/16/07
Re: Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)
Posted: Jul 6, 2012 3:58 PM   in response to: sartaj in response to: sartaj
Click to report abuse...   Click to reply to this thread Reply
sartaj

Posts: 2
Registered: 07/06/12
Re: Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)
Posted: Jul 9, 2012 1:51 AM   in response to: DaveHornbeck in response to: DaveHornbeck
Click to report abuse...   Click to reply to this thread Reply
1. Does the auto-detect not work for a clustered sc-fdma signal?
2. Do I need to set in two users to analyse a clustered sc-fdma signal because for a single user I am unable to set in non-contiguous resource allocation in the LTE resource allocator.
DaveHornbeck

Posts: 65
Registered: 03/16/07
Re: Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)
Posted: Jul 16, 2012 4:20 PM   in response to: sartaj in response to: sartaj
Click to report abuse...   Click to reply to this thread Reply
Auto detection cannot be used for clustered sc-fdma waveforms.
You do not need multiple users but you must configure multiple allocations as shown in the attached picture.

Point your RSS reader here for a feed of the latest messages in all forums