Contact an Expert

Thread: Two simulated network using 8960 series 10 in a shield box


Permlink Replies: 2 - Pages: 1 - Last Post: Jul 10, 2012 7:57 AM Last Post By: ernesto_dan
ernesto_dan

Posts: 5
Registered: 08/16/11
Two simulated network using 8960 series 10 in a shield box
Posted: Jul 5, 2012 2:58 PM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I have the test environment below:

  • Two E5515E 8960 Series 10
  • One N9360A-S04 RF Shield Box

I would like to combine both 8960 RF signal to connect to the shield box RF input and simulate two different GSM/UMTS networks serving a cell phone device.

The question is: can I use "11636A Power Divider" for this purpose? If not, what accessory can be used?

Attached is the environment diagram that I want to setup.

Thanks in advance,

Ernesto Dan
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Two simulated network using 8960 series 10 in a shield box
Posted: Jul 9, 2012 2:17 PM   in response to: ernesto_dan in response to: ernesto_dan
Click to report abuse...   Click to reply to this thread Reply
Hi Ernesto Dan -

The 11636A should be fine.

For further information, tips and troubleshooting, I suggest you start at the online user guide for Two-Cell test systems:
http://wireless.agilent.com/rfcomms/refdocs/wcdma/wcdma_gen_bse_two_cell_test_system.html

Regards -
ernesto_dan

Posts: 5
Registered: 08/16/11
Re: Two simulated network using 8960 series 10 in a shield box
Posted: Jul 10, 2012 7:57 AM   in response to: tabbott in response to: tabbott
Click to report abuse...   Click to reply to this thread Reply
Hi tabbott,

Thanks for your answer and extra info, it will be very useful.

Best regards,

Ernesto Dan

Point your RSS reader here for a feed of the latest messages in all forums