Contact an Expert

Thread: Phase Change Timing


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 14, 2012 1:23 PM Last Post By: tabbott
bri

Posts: 1
Registered: 06/13/12
Phase Change Timing
Posted: Jun 13, 2012 10:00 AM
Click to report abuse...   Click to reply to this thread Reply
I need help making a measurement.

I have a N5181A MXG feeding into a N9020A MXA. I want to change the phase of the signal and detect how long it takes from, issuing the phase change until it is detected by the MXA. This will give me the external time, so when I measure group delay in a receiver I can subtract the external time.

I am not even sure I can do this, how to do this, or if I have the right equipment or options. I am at a loss at this point.

Thanks
Brian
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Phase Change Timing
Posted: Jun 14, 2012 1:23 PM   in response to: bri in response to: bri
Click to report abuse...   Click to reply to this thread Reply
Hi Brian -

You will want to use the IQ Analyzer mode in the MXA. The IQ Waveform measurement will allow you to capture the signal over a specified bandwidth and measurement interval. You can then trigger the measurement and acquire the signal with your phase change applied to the signal. Once you acquired the data with a READ:WAV0? you will have the IQ data of your input signal. By calculating the arctan(I/Q) you will have the relative phase of the signal to the MXA. You can then determine at what sample your phase change occurred and determine from this what time interval it occurred. You can use a simple pulse signal to determine the trigger delay needed to calibrate the system to account for cable and trigger time uncertainties.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums