Contact an Expert

Thread: How measure the electrical length with HP 8719C VNA?


Permlink Replies: 18 - Pages: 2 [ Previous | 1 2 ] - Last Post: Apr 30, 2012 7:45 AM Last Post By: Dr_joel
neogsj

Posts: 12
Registered: 11/08/11
Re: How measure the electrical length with HP 8719C VNA?
Posted: Apr 25, 2012 8:41 AM   in response to: Dr_joel in response to: Dr_joel
Click to report abuse...   Click to reply to this thread Reply
Dr_joel wrote:
The trouble here is you are using electrical delay to do a "port extension" function, which is the cause of your problems. You can use electrical delay to remove delay from a measurement, and it will have 2:1 phase response for reflection measurments and 1:1 for transmission. But that is not the proper function to use. If you use port extension to remove delay from your measurement then it automatically accounts for relfection vs. transmission measurment. Stop using electrical delay and try port extensions for this purpose. I think you will find your troubles go away.

I tried to measure the DUT without normalization with using port extension. By input 36 ps or 18 ps in Extension input A, I still do not have correct phase result for S11. (in the link http://www.vnahelp.com/tip9.html, it says I should use 18 ps to achieve 36 ps ED for S11)

Then, I measured the DUT with normalization. By input 18 ps in Extension input A, I can have correct phase result for S11 now.

But I am still confused by the normalization, electrical delay and port extension even I have the correct phase result now. Is the last method by which I can have good result is correct?
Dr_joel


Posts: 2,788
Registered: 12/01/05
Re: How measure the electrical length with HP 8719C VNA?
Posted: Apr 25, 2012 10:26 PM   in response to: neogsj in response to: neogsj
Click to report abuse...   Click to reply to this thread Reply
Still not doing it right. Don't use extension A or B. Use PORT 1 extension or Port 2 extension, as you are extending the test port, not the receiver.
neogsj

Posts: 12
Registered: 11/08/11
Re: How measure the electrical length with HP 8719C VNA?
Posted: Apr 26, 2012 12:57 PM   in response to: Dr_joel in response to: Dr_joel
Click to report abuse...   Click to reply to this thread Reply
Dr_joel wrote:
Still not doing it right. Don't use extension A or B. Use PORT 1 extension or Port 2 extension, as you are extending the test port, not the receiver.

But when I input 18ps (half electrical length of single connector) or 36 ps (electrical length of single connector) in Port 1 extensions, I can not have measured result similar as the simulation (10 degree difference) with or without the normalization.
Dr_joel


Posts: 2,788
Registered: 12/01/05
Re: How measure the electrical length with HP 8719C VNA?
Posted: Apr 30, 2012 7:45 AM   in response to: neogsj in response to: neogsj
Click to report abuse...   Click to reply to this thread Reply
If you want to measure the delay of a DUT with an SMA connector, using S11, then you must do a calibration without a 3.5 mm calibration kit, don't do any normalization.

Measure S11, put up a "delay" trace and use trace statisitics to measure the mean value.

Remember that your DUT can have radiation and fringing that can add phase rotation, increasing the apparent delay.

Don't use port extension on A, use port 1 (extension on A is intended to be used when cables are added behind the directional coupler). Just because it gives an answer you like, doesn't mean it is the correct method.

Remember that your simulation is not the real thing. No reason the simulation should match the DUT response if the simulation is not correct.

Point your RSS reader here for a feed of the latest messages in all forums