이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

16500B Operating System Software (Version 3.14)

These files contain the 3.14 OP SYS for the 16500B and are dated 07/18/97. (Note: These are DOS files. DO NOT use the lifutil to copy.)

All files on these 5 disks should be copied into the '\SYSTEM' directory on the 16500B hard disk drive.

The 3.14 version is the same as the 3.13 version except for the 'SYS_034' file which has been updated to support the E2474A. If you/customer already has version 3.13 installed...just 'get' the 'SYS_034' (on Disk #4) file and copy it over the existing 'SYS_034' file on the 16500B Hard Drive.

Version 3.14 or later of the 16500B operating system is required to work with the the E2474A.

릴리스 날짜 버젼 버전 설명
1997-08-04 3.14 Operating system software files for the 16500B logic analysis system.

다운로드 방법

  • Click the download button, select file and save.

설치 방법

  • See Documentation

라이센스

  • 라이센스 필요 없음
다운로드

설치 위치:

Instrument

사전 조건

  • 사용 가능한 정보 없음

지원되는 계측기

  • 16500B